Whether in bustling cities or developing regions, prosperity and progress in our modern society are inconceivable without energy. Energy is the driving force and lifeline of our civilization – in households as much as in industry, transportation or healthcare.
One of the greatest challenges of the 21st century is to supply the required energy efficiently, economically, and with minimal impact on the environment – a challenge that involves the entire chain of energy logistics from generation to transportation and distribution.
These efforts will be affected by four major factors in the coming decades: worldwide growth in energy demand, increasing urbanization, dwindling fossil energy resources, and the effects of climate change.
Power network operators around the globe are investing knowledge and capital to meet these new challenges. Success will depend on a number of factors, including optimized utilization of existing resources and networks, further expansion of infrastructures, and integration of decentralized and regenerative energy production with renewables.
Energy automation plays an important role in this increasingly complex landscape. It facilitates improved energy management, more flexible responses to changing demands, and increased efficiency throughout the networks – all of which ensures a high level of energy reliability at reduced cost.
How can I fight blackout before it happens?
With QuickStab - a system-wide voltage and steady-state stability index calculation
The ability to transfer energy across AC networks is hampered by thermal, voltage and stability limits. The maximum loadability of a transmission system is the state where voltages collapse and units may get out of synchronism, and is a severe constraint.
The distance from a given operating point to the state of maximum loadability is called stability reserve. It changes when the system state has changed, and may be quite different from values computed offline. Its recalculation after each state estimate and load-flow is required because operating the system near its stability limit may lead to blackouts. This problem is solved rapidly by QuickStab®.
Given a load-flow solution or state estimate of a multi-area power system, QuickStab®:
QuickStab® can be used
The input data required by QuickStab® include the following:
The input base-case can be supplied in industry-standard formats including:
Starting from a solved multi-area power-flow base case, the voltage / steady-state stability analysis performed by QuickStab® encompasses the following major steps:
The elapsed time for running QuickStab is less than, or equal to, one (1) second when performing system-wide voltage and steady-state stability calculations for a power system network comprising about 2,000 buses on a regular PC.
QuickStab quantifies the risk of blackout, is extremely fast, can help develop preventative and corrective strategies, and makes extensive use of intuitive graphics.
The ability to quickly assess the distance to instability and the impact of generators on stability is paramount for fast and reliable decision-making and it helps the Transmission System Operator (TSO) to:
The program’s capability to setup and assess multi-area what-if scenarios is another useful and quite unique benefit. Knowledge is power – and the ability to quickly determine the actual transfer limits of each and any sub-area of the transmission system will offer the TSO a strategic edge in the extremely competitive electricity market.