The growth of cities will be a dominant demographic trend of coming decades. The current proportion of the world‘s population living in urban areas just passed the halfway mark. The United Nations expects it to rise to almost 60% by 2025, and to reach 70% around 2050.
As cities grow, personal living conditions in cities become more important. Energy supply, whether electricity, steam, hot water or chilled water, will, in the future, place major challenges on infrastructure. Modern architectural design generates a rapidly growing cooling demand.
Siemens Cooling Solution Generates 10,000 Tons of Refrigeration
The Siemens Refrigeration Compressor Package (SRCP) is equipped with two highly efficient compressors, generating 10,000 tons of refrigeration (RT). Both engineering and construction companies benefit from the space-saving effect of the SRCP. Space is money, especially when the district cooling plant is located in the middle of the city.
There are many reasons for this growing cooling demand , including:
Cooling Plant Reduces Greenhouse Gas
A survey among 522 stakeholders in 25 large, urban agglomerations worldwide indicates the willingness to invest in an improved environment. There‘s a strong interest in megacities to reduce greenhouse gas emissions and other air pollutants – megacities already emit roughly 10% of global CO2 emissions.
A district cooling plant offers a perfect alternative to conventional window A/C, since the cooling capacity is generated in an effective and efficient manner. A central district cooling plant generates cool water and distributes it through a network of piping system to individual customer buildings. District cooling has been implemented in a variety of structures, both private and government-owned utilities, universities and airports. The district cooling systems serve a wide variety of types of buildings, including:
The benefits of district cooling are:
A switch from window A/C to an efficient district cooling plant with the Siemens Refrigeration Compressor Package (SRCP 10) is like reducing the related emissions from 70 thousand cars to 30 thousand cars. Using the electrical power generated by a Siemens solar thermal power plant, eliminates the emissions completely.
Features of the Siemens Compressor Chiller Package:
Advantages of the Siemens Compressor Chiller Package:
Implementation
The cooling demand in cities is directly correlated to the impact of the sun, in other words the load profile of a district cooling plant varies drastically from day to night.
To compensate for the varying refrigeration demand, a combination of the Siemens Refrigeration Compressor Package with smaller chiller equipment is feasible.
Siemens has secured orders for 45 steam turbines for solar thermal power plants: