As a pioneer in air-insulated and gas-insulated switchgear, Siemens has 25 years of know-how in the development of switchgear and switching devices. Customers can take full advantage of this technology. Since the power demand for processes in the oil & gas industry is increasing, Siemens Energy is covering this high rated-current and short-circuits demand with air-insulated (up to 38 kV) and gas-insulated medium-voltage (MV) switchgear (up to 40.5 kV).
The MV gas-insulated switchgear at a glance:
The MV air-insulated switchgear at a glance:
The Siemens low-voltage (LV) switchboard has a modular design with high combination flexibility. Adaptations for new performance demands during operation can be carried out easily by exchanging the withdrawable units or changing the compartments. The LV switchboard is available in a fixed-mounted, plug-in and fully withdrawable design and as a Motor Control Centre (MCC).
Global capabilities for switchgear and switchboard
Siemens has global engineering and manufacturing capabilities for our medium-voltage and low-voltage switchgear and switchboard and holds important approvals and certifications for onshore and offshore applications in oil and gas.
SIPLINK, power transmission and power distribution
In this section you will also find information on SIPLINK and its application on drill ships to create fault-tolerant power supply systems for the thrusters to avoid drift-off of the ship. This keeps stability of the power plant high and in the event of a black-out brings power back to the thrusters within approximately 17 seconds. Additionally, there is a general overview of the Siemens portfolio in power transmission and power distribution products, systems and solutions in our Power Engineering Guide.
Siemens Power Engineering Guide, a useful tool for anyone involved in the transmission or distribution of electrical energy.
Click to continue
The combination of high reliability, a compact and low weight design, low operating costs and smooth and efficient installation and commissioning have led Siemens gas-insulated switchgear products to be used in over 500,000 panels worldwide.
Click to continue
The geographical spread of the 14 worldwide Siemens air-insulated switchgear manufacturing sites ensures not just close proximity to our customers, but also that our air-insulated switchgears are manufactured to meet all local as well as international standards.
Click to continue
SIPLINK provides a means of interlinking power generators or networks which have different frequencies or power capacities without impairing system stability or increasing the fault currents.
Click to continue
Siemens integrated products and systems ensure flexible and economical power distribution over the entire life cycle.
Click to continue
City Network Ulm “SIPLINK for Peak Load Exchange”, Germany
A new system for the city power districts was required to permit connection of different energy suppliers and networks, Siemens selected its SIPLINK (Siemens Multifunctional Power Link) system. Siemens’ scope of supply:
Transocean – new enterprise class, Korea
A fail-safe energy supply for the consumer and a decrease in the number of running generators in low load mode were required. Siemens E D MV 3 developed a solution with inverters, which can provide energy from two different sources. Siemens’ scope of supply:
Brochure: Gas-insulated medium-voltage switchgear
Flyer: What's behind GIS?
Brochure: Air-insulated medium-voltage switchgear
SIPLINK Brochures:
LV Switchboards and MCCs
Publications