Powergrid Corporation of India, Limited, an Indian government entity, is the only agency responsible for transmission of power across the country. In its current five-year plan, the Indian government has set the target “Power for All by 2012”. In India, where efficiency of power transmission is now approximately 52 %, the enhancement of transmission capacity will play a vital role in achieving the target.
The project focuses on the enhancement of the transmission capacity of the northern grid. Sites are at Lucknow, Bareilly, and Unnao, in the state of Uttar Pradesh. Unnao Substation belongs to the Uttar Pradesh state government, while Lucknow and Bareilly belong to Powergrid. The Bareilly FSC plant will have local control as well as remote control from Powergrid’s Lucknow Substation.
| Customer | Powergrid Corporation of India, Ltd. |
| Project Name | Fixed Series Compensation at Lucknow, Bareilly, and Unnao substations associated with enhancement of transmission capacity in the east-west corridor of the northern region |
| Location | 400 kV Gorakhpur-Lucknow lines at Lucknow Substation 400 kV Bareilly-Mandolla lines at Bareilly Substation 400 kV Unnao-Bareilly lines at Unnao Substation |
| System | Fixed Series Capacitor |
| Capacitor Rating | 2 x 189 Mvar FSCs1) 2 x 187 Mvar FSCs2) 2 x 311 Mvar FSCs3) |
| Compensation Degree | 30 %1) 30 %2) 45 %3) |
| Digital control system | Simatic TDC |
1) Lucknow
2) Bareilly
3) Unnao
The major part of Brazil’s energy is generated by hydroelectric power plants. The hydrographic conditions in the North of Brazil possess large capability for generating hydroelectric power to cover the energy demand in the South.
In 2006, after the first two North-South Interconnection lines from the years before had proved successfully, the Brazilian Electricity Regulatory Agency (ANEEL) awarded a third parallel line, North South Interconnection III. In the middle section of the transmission line from Colinas (Tocantis) down to Serra da Mesa II (Goiás) power had to be transmitted over an enormous distance of 696 km. This Lot B, the longest part of the three Lots, was awarded to INTESA, a consortium of Eletronorte, Chesf, Engevix and a private investor. To avoid losses and voltage stability problems in Lot B Siemens supplied in a consortium with Areva five Fixed Series Capacitors (FSCs), Line Protection and substation HV equipment. Siemens as the consortium leader installed four FSCs at Eletronorte´s substations Colinas, Miracema and Gurupi and one at Furnas´ substation Peixe II within a delivery time of 14 months. So an interconnection between north and south was indispensable.
Due to high complexity of power grids, the degree of line compensation had to be determined carefully for each section. The degree of line compensation should definitely be as high as possible. However, if it exceeds 70%, sub synchronous resonances appear whereas these have to be avoided. By means of this, these substations were constituted to install the FSCs with ratings shown in the table:
| Customer | Brazilian Electricity Regulatory Agency (ANEEL) |
| Project Name | North South Interconnection III |
| Location | In Eletronorte´s substations in Colinas, Miracema and Gurupi In Furnas´ substation Peixe II |
| System | Fixed Series Capacitor |
| Capacitor Rating | 200 MVAr FSC at Colinas 2 x 194 MVAr FSCs at Miracema and Gurupi 130 MVAr FSC at Gurupi 343 MVAr FSC at Peixe II |
| Compensation Degree | 51 % Colinas 70 % Miracema and Gurupi 70 % Gurupi 68 % Peixe II |
| MOV Data |
|
| Digital control and protection system |
In summer of 2005, Siemens was awarded the Fengjie Series Compensation System located in Wanzhou 500 kV ac-network, Fengjie County, Wanzhou District. Fixed Series Compensation (FSC) was found as the appropriate solution for an increase of power transfer capability with the existing lines and to stabilize the interconnected networks by reducing the connecting line impedance.
The Fengjie 500 kV Series Capacitor Station is about 130 km away from Wanxian substation where one of the two 500 kV lines of Chuanyu Grid-to-Central China Mains interconnection project starts. Within this project, planned by the State Grid Corporation of China, Fenjie 500 kV Series Compensation Station is an important asset. It has a capacity of 2x610 MVar and a compensation level of 35%. Its FSC system consists of two capacitors, one in each of the parallel lines located in Fengjie substation. Over a distance of 360 km it connects Wanxian substation in the west with the Longquan substation in the east.
| Customer | State Grid Corporation of China |
| Project Name | Fengjie |
| Location | Fengjie County, Wanzhou District, Chongquing City |
| System | Fixed Series Capacitor |
| Capacitor Rating | 35.3 Ohm/2 x 610 MVAr |
| Compensation Degree | 35 % |
| MOV Data | 35 MJ MOV total energy capability 500 kV |
| Digital control and protection system |
In September 2004 Siemens succeeded in winning the contract for the refurbishment of two series capacitor installations at Edisons Eldorado Substation southwest of Boulder City, Nevada. As a result of new power generation installed in the Las Vegas area the fault duty on the 500 kV transmission network is above the design ratings of the existing equip-ment and therefore the two series capacitors “Lugo” and “Moenkopi” at the Eldorado Substation need to be replaced.
It is the intention to increase the power transfer between Arizona / Nevada and Southern California within the next few years. The so called Eldorado-Moenkopi SC is in series with the transmission line leading to the Moenkopi subsation in Arizona and the Eldorado-Lugo SC is in series with the transmission line leading to the Lugo substation in Southern California. The Lugo series capacitor installation will consist of two segments, one segment will be a FSC and the other segment will be a TPSC. The Moenkopi series capacitor installation will consist of three segments, two segments will be FSCs and the other segment will be a TPSC. The Lugo FSC is in service since March 15th 2006 and the Moenkopi FSC since June 1st 2006.
| Customer | Southern California Edison (SCE) |
| Project Name | Eldorado |
| Location | Near Boulder City, NV, USA |
| Capacitor Rating | 199 Mvar / segment1) 162 Mvar / segment2) |
| Compensation Degree | 17,5 % / segment1) 11,7 % / segment2) |
| Digital control and protection system | SIMADYN D® |
1) Lugo
2) Moenkopi
In August 2002 Siemens succeeded in winning a series capacitor contract with Dominion Virginia Power.
To accommodate increased power generation at the Bath County Pumping Station, Dominion had to add two series capacitors to the Virginia 500 kV network in the Bath County Area. Each of the two transmission lines from the Bath County Pumping Station, one leading to the Lexington substation and the other leading to the Valley substation have been equipped with a fixed series capacitor of 60 % compensation level.
The Valley FSC has been in commercial operation since November 13th 2003 and the Lexington FSC has been in commercial operation since December 2nd 2003.
| Customer | Dominion Virginia Power |
| Project Name | Lexington & Valley FSCs |
| Location | Near Rockbridge Bath, Virginia1) And near Weyers Cave, Virginia2) |
| Capacitor Rating | 13.1 Ohm / 355 Mvar at 3 kA1) 18.7 Ohm / 505 Mvar at 3 kA2) |
| Compensation Degree | 60 %1) 60 %2) |
| Digital control and protection system | Siemens SIMADYN D® |
1) Lexington
2) Valley
In May 2002, Siemens received the turnkey contract from OTRACO to install two series capacitor banks in the MOTRACO network. MOTRACO is an independent transmission company owned in equal shares by three utilities: EdM from Mozambique, SEB from Swaziland and ESKOM from South Africa. The MOTRACO network consists of two 400 kV transmission lines from ESKOM (Camden and Arnot substation) to the Maputo substation. The transmission line from Camden to Maputo is intersected by a 400 kV busbar in Swaziland at Edwaleni II substation.
The bulk of the energy which is transferred via these transmission lines is for the Mozal aluminum smelter in Maputo. The capacity of the aluminum smelter will be increased. Therefore also the lines have to be upgraded to cope with the increased power demand. As part of this upgrade, Siemens supplies the two fixed series capacitor banks. One bank is installed directly in Maputo substation in the Edwaleni-Maputo line. The second FSC is installed in Barberton substation approximately halfway between Arnot power station and Maputo substation close to the city of Barberton, in the Republic of South Africa. Both FSCs have been in commercial operation since mid April 2003.
| Customer | MOTRACO |
| Project Name | Maputo FSC Barberton FSC |
| Location | Maputo, Mozal substation, Mozambique1) Barberton substation, near Nelspruit, in the Republic of South Africa2) |
| Capacitor Rating | 28.44 Ohm / 344 Mvar1) 44.24 Ohm / 535 Mvar2) |
| Compensation Degree | 50 %1) 50 %2) |
| Digital control and protection system | Siemens SIMADYN D® |
1) Maputo FSC
2) Barberton FSC
Part of New York's electric energy is supplied by Hydro-Québec, from the hydroelectric power plant "Churchill Falls" on the coast of Labrador in Newfoundland. To increase the transferable power of the 735-kV transmission line from the power plant Churchill Falls to Montreal - a distance of about 1200 km, Hydro-Québec decided to install three 3-phase series capacitors at the Montagnais substation in the Canadian province Québec.
From Montreal, some of the electricity is transmitted via the HVDC back-to-back link at Chateauguay in Canada to the network operated by the New York Power Administration in the USA. Montagnais is one of the most important facilities in Hydro-Québec's eastern power network, because it is not far away from the generators in Churchill Falls.
In 1993, Hydro-Québec placed an order with Siemens for the supply and installation of the three series capacitors, because Siemens was able to fulfill the special technical demand in accuracy and reaction time needed for the extreme conditions in the Canadian winter. Siemens was also the first manufacturer whose surge arresters succeeded in withstanding Hydro-Québec's extra tough pressure relief tests for the 735-kV application, involving a full discharge of a specially set-up bank of original capacitors.
The Montagnais series capacitor is able to withstand the extreme temperatures from -50 °C to +40 °C. The series capacitor installation helps to improve the transmission line stability and is able to compensate up to 40% of the inductive line impedance, thus enhancing the transferable power to 6000 MVA.
| Customer | Hydro-Québec (HQ) |
| Project Name | Montagnais FSC |
| Location | Poste Montagnais, Canada North East Network |
| Capacitor Rating | 30 Ohm / 1500 Mvar (3 x 476 MVAr) at 2.= kA |
| Compensation Degree | 40 % |
| MOV Data | 40 kA MOV current 44 MJ MOV energy capability 252 kV protective level |
| Digital control and protection system | Siemens SIMADYN D® |
Brazil's national energy holding Electrobrás had planned to connect the northern with the southern power networks for a long time. Finally, the heavy increasing demand for electric energy in the south decided the issue to build the North-South Interconnection line.
The network in the south, south-east, central and mid west regions supplies energy to the area of the country south of the capital, Brasilia, and the network in the north and northeast provides energy to the areas north-east of Bahia to Belém on the Amazon delta.
Most of the electric power of both networks is generated in hydroelectric power plants, for example from the power plant Xingó at the Sao Francisco river. The backbone of the interconnection line is the 500-kV transmission line from Imperatriz to Serra da Mesa. The North-South Interconnection, with its capacity of 1300 MW, enables a more flexible expansion of the hydroelectric power plants along the Tocantins river. To increase the energy transmission capacity and to stabilize the system Electrobrás decided to use Flexible AC Transmission Systems. In 1997, Siemens received the order from FURNAS to supply one TCSC with the mentioned above data.
| Customer | FURNAS – Centrais Elétricas S.A. |
| Project Name | Serra da Mesa (SdM) |
| Location | North of Brasilia, Brazil |
| System | Thyristor-Protected Series Capacitor |
| Capacitor Rating | 13.27 Ohm (blocked valve) and 15.92 Ohm (TCSC)/107.46 MVAr at 1.5 kA |
| Compensation Degree | 5-6 % (continuous) 7-15% (temporary) |
| TCR Data | 100 mm Ø 5.5 kV electrically triggered thyristors 23.9 kV nominal valve voltage at 3.55 kA 1.123 MJ Valve MOV 87.3 kV protective level |
| MOV Data | 22.46 MJ MOV energy capability 27.2 kA peak MOV current at protective level 89.8 kV/2.65 pu protective level |
| Digital control and protection system | SIMADYN D® |