Siemens is erecting HelWin 2, the link between the North Sea offshore windfarm Amrumbank West and the onshore grid. The customer is TenneT TSO GmbH of Bayreuth, Germany.
The grid connection, designed as a high-voltage direct-current transmission link, has a rating of 690 megawatts (MW) and is scheduled to be operational by 2015. Amrumbank West will be built in the North Sea, about 55 kilometers from the mainland, 35 kilometers north of Helgoland, and 37 kilometers west of the North Frisian island of Amrum. The wind farm will have a power capacity between 300 and 400 MW. Together with the Meerwind and North Sea East offshore windfarms, Amrumbank West is part of the North Sea cluster HelWin.
| Customer | TenneT, Germany |
| Project name | HelWin2 |
| Location | 131 km on-/offshore cable Büttel, Germany |
| Power Rating | 690 MW |
| Voltage Levels | 155 kV/300 kV/380 kV, AC ±320 kV, DC |
| Equipment | HVDC PLUS 2 x transformers 4 x AC cable compensation reactors High-voltage gas-insulated switchgear GIS |
| Type of plant | WIPOS offshore platform (self-lifting) with HVDC PLUS |
Siemens will supply the world’s largest voltage-sourced converter (VSC) offshore system with a rating of 864 MW for the SylWin1 project. Siemens’ HVDC PLUS link will connect the Dan Tysk wind farm to the German shore. The converter will be installed on an offshore platform, where the voltage level will be stepped up and converted to ±320 kV DC. The platform will accommodate all electrical equipment required for the HVDC converter station: two transformers, four AC cable compensation reactors, and high-voltage gas-insulated switchgear (GIS). Similar to the BorWin2 and HelWin1 projects, the Siemens wind power offshore substation (WIPOS®) will be designed as a floating, self-lifting platform. The energy will be transmitted via subsea and land cable to Büttel, where an onshore converter station will reconvert the DC to AC and feed it into the 380 kV AC grid. The transmission link is scheduled to start operation in 2014.
| Customer | TenneT, Germany |
| Project name | SylWin1 |
| Location | 210 km on-/offshore cable Büttel, Germany |
| Power Rating | 864 MW |
| Voltage Levels | 155 kV/300 kV/380 kV, AC ±320 kV, DC |
| Equipment | HVDC PLUS 2 x transformers 4 x AC cable compensation reactors High-voltage gas-insulated switchgear GIS |
| Type of plant | WIPOS offshore platform (self-lifting) with HVDC PLUS |
The Gwynt y Môr project, situated in the Liverpool Bay area around 18 kilometers off the English northwest coast, will have a generating capacity of 576 MW upon completion. The project will be developed by a joint venture between RWE Innogy, Stadtwerke München, and Siemens. Siemens will be responsible for connecting the wind farm to the grid as well as delivering all 160 Siemens 3.6 MW class wind turbines. The turbines will be installed in water depths between 15 and 30 m. The grid connection of Gwynt y Môr will consist of two offshore substations, each equipped with two 33/132 kV 160 MVA transformers. In order to meet grid code requirements, Siemens will install two ±50 MVAr SVC PLUS systems for reactive power compensation as part of the onshore substation connection.
| Customer | RWE Innogy, Germany |
| Project name | Gwynt y Môr |
| Location | Liverpool Bay, 18km off the North Wales coast, UK; St. Asaph, Wales |
| Power Rating | 576 MW |
| Voltage levels | 33 kV / 132 kV, AC; 11 bays |
| Equipment | 2 x Offshore Substations, each with: 2 x 160 MVA transformers (33/132 kV) 2 bays 132 kV GIS switchgear 10 bays 33 kV switchgear Onshore Substation: 2 x SVC-PLUS-systems 3 x 320 MVA transformers(400kV/132kV/13,9kV) 2 x 132 kV harmonic filters (40 MVAr) 11 bays 132 kV GIS switchgear Power Cabling: 2 x circuits 400 kV & 7 x circuits 132 kV onshore power cable |
| Type of plant | Two offshore substations; Onshore substation with SVC PLUS |
| Number of wind turbines | 160, each 3.6 MW |
Siemens Energy has been contracted by RWE Innogy in August 2010 to supply the offshore substation for their wind farm „Nordsee Ost“ project which is going to be located in the Northsea 33 kilometers northeast from the island Helgoland in Germany. The offshore substation is provided at a platform which is going to be installed on a 39 m high steel structure. The offshore AC substation collects the generated 295 MW wind power. It allows high voltage AC power supply by transferring the voltage from 33 kV to 155 kV via transformers. Subsea cables will transmit the wind power to HVDC platform "HelWin". Power supply is scheduled first for summer 2012. The wind farm „Nordsee Ost“ is going to provide 295 tausend households with green power when it is totally energized in 2013.
| Customer | RWE Innogy, Germany |
| Project name | Nordsee Ost |
| Location | 33 km north-east of Helgoland, North Sea, Germany |
| Power Rating | 295 MW |
| Voltage levels | 33 kV / 155 kV, AC |
| Equipment | GIS 8DN9 180 MW transformers (33/155 kV) |
| Type of plant | Offshore substation |
| Number of wind turbines | 48, each appr. 6.15 MW |
For the project HelWin1, Siemens will be supplying a voltage-sourced converter (VSC) system with a rating of 576 MW using Siemens HVDC PLUS technology. The wind farms Nordsee Ost and Meerwind are designed to generate 576 MW and will be connected through a Siemens’ HVDC PLUS link to shore. The converter will be installed on an offshore platform, where the voltage level will be stepped up from 155 to 250 kV and then converted to DC at the same voltage level. The platform will accommodate all the requisite electrical high-voltage AC and DC equipment for the converter station. Similar to the Borwin2 project, the Siemens wind power offshore substation (WIPOS) will also be designed as a floating, self-lifting platform. Energy will be transmitted via subsea and land cable to Büttel, northwest of Hamburg, Germany, where an onshore converter station will reconvert the DC back to AC and transmit it into the grid. The entire transmission link and grid connection is expected to be in operation by 2013.
| Customer | transpower offshore gmbh, Germany |
| Project name | HelWin1 |
| Location | Offshore: 85km offshore north-west of Helgoland, North Sea, Germany; Onshore: Büttel (north-west of Hamburg), Germany |
| Power Rating | 576 MW |
| Voltage levels | 155 kV to 250 kV, AC; 259 kV, DC |
| Equipment | HVDC PLUS 1 x HVDC PLUS 2 x 155/250 kV transformers GIS |
| Type of plant | WIPOS offshore platform (floating & self-lifting) with HVDC PLUS; Onshore HVDC PLUS |
For the BorWin2 project, Siemens will supply the voltage-sourced converter (VSC) system – using Siemens HVDC PLUS technology – with a rating of 800 MW. The wind farms Veja Mate and Global Tech 1 are designed to generate 800 MW and will be connected through Siemens’ HVDC PLUS link to shore. The converter will be installed on an offshore platform, where the voltage level will be stepped up from 155 to 300 kV AC and then converted to DC at the same voltage level. The platform will accommodate all the requisite electrical equipment for the HVDC converter station, two transformers, four AC cable compensation reactors and high-voltage gas-insulated switchgears (GIS). The Siemens wind power offshore substation (WIPOS) will be designed as a floating, self-lifting platform. Energy will be transmitted via subsea and land cable to Diele close to Papenburg, where an onshore converter station will reconvert the DC back to AC and feed it into the 400 kV AC network. The entire transmission link is expected to begin operation in 2013.
| Customer | transpower offshore gmbh, Germany |
| Project name | BorWIn2 |
| Location | Offshore: 96 km offshore – NNW of the island Borkum, Germany Onshore: Diele, Germany |
| Power Rating | 800 MW |
| Voltage levels | 155 kV / 300 kV / 400 kV, AC; 300 kV, DC |
| Equipment | HVDC PLUS 2 x transformers 4 x AC cable compensation reactors; High-voltage gas-insulated switchgear GIS Cable routes: HVDC cable: 200 km (total), thereof 125 km offshore (incl. Watten Sea) and 75 km onshore HVAC cable: connection to “Veja Mate”: 10 km connection to “GlobalTech 1”: 30 km |
| Type of plant | WIPOS offshore platform (floating & self-lifting) with HVDC PLUS; Onshore substation HVDC PLUS |
The Lincs project, a wind farm owned by Lincs Windfarm Limited, whose shareholders include Centrica, DONG, and Siemens, will be located in the Greater Wash region approximately eight kilometers from Skegness, Lincolnshire, UK. Lincs will have a generating capacity of 270 MW employing 75 Siemens 3.6 MW wind turbines installed in water depths of between eight and 18 meters. In addition to supplying the wind turbines Siemens will be providing performance studies and constructing the offshore substation topside housing two 33/132 kV 240 MVA transformers as well as the onshore AC substation for this project. This contract award follows the successful commissioning of Centrica’s Lynn & Inner Dowsing offshore wind farms, for which Siemens also provided the grid connection.
| Customer | Lincs Wind Farm Ltd, UK |
| Project name | Lincs |
| Location | 8 km offshore, near Skegness, Lincolnshire, UK |
| Power Rating | 270 MW |
| Voltage levels | 33 kV / 132 kV / 400 kV, AC |
| Equipment | Offshore Substation: 2 x 240 MVA transformers (33/132 kV) 2 x 33 kV shunt reactors (40 MVAr) 4 bays 132 kV high-voltage switchgear 12 bays 33 kV medium-voltage switchgear Onshore Substation: 1 x SVC PLUS 2 x 300 MVA, power transformers (400 kV / 132 kV / 13,9 kV) 2 x 132 kV shunt reactors (40 MVAr) 2 x 132 kV harmonic filters (30 MVAr) 7 bays 132 kV GIS and 1 bay 400 kV switchgear Power Cabling: 12 km double circuit 132 kV onshore power cable |
| Type of plant | Offshore substation: conventional topside / jacket. Onshore subtation with SVC PLUS |
| Number of wind turbines | 75, each 3.6 MW |
Situated 24 kilometers from Clacton-on-Sea, Essex, the development of this project will upon completion of phase one and two generate 1,000 MW of green power and will be the world’s largest offshore wind farm when it is energized in 2012.
In phase one, two offshore substations will be delivered to collect the 630 MW of power generated by 175 Siemens wind turbines before transferring the power to shore via the main 150 kV export cables.
Siemens is the design-build contractor responsible for the overall electrical design of the grid connection providing performance studies, the equipment for two offshore substations, the complete onshore substation, and reactive power compensation.
| Customer | Dong Energy, E.ON and Masdar, UK |
| Project name | London Array |
| Location | 24km from Clacton-on-Sea, Essex, UK |
| Power Rating | 630 MW (1000 MW) |
| Voltage levels | 150 kV, AC |
| Type of plant | 2 x Offshore substatins; onshore substatition with SVC PLUS |
| Number of wind turbines | 175, each 3.6 MW |
Roughly 25 kilometers off the coast of Suffolk, 140 Siemens wind turbines, 3.6 MW each, will produce carbon-free electricity. Two 33/132 kV offshore Siemens substations with two 90 MVA transformers on one and three 180 MVA transformers on the other will help export the electricity through three three-phase 132 kV XLPE submarine cables. Near the network point-of-coupling to the grid in the village of Sizewell, Siemens is also installing a reactive power compensation device, which allows the wind farm to meet the requirements of the UK grid code.
| Customer | Greater Gabbard Offshore Winds Ltd., U.K. |
| Project name | Greater Gabbard |
| Location | North Sea, close to the Thames Estuary and Sizewell Village, Suffolk, UK |
| Power Rating | 500 MW |
| Voltage levels | 13,9 kV / 33 kV / 132 kV, AC |
| Equipment | 3 x SVC PLUS 3 x 180 MVA transformers (33/132 kV) 2 x 90 MVA transformers 3 x three-phase 132 kV XLPE cable 3 x 132 kV HIS, 13,9 kV GIS, 33 kV GIS Mechanical switched Capacitors and Reactors |
| Type of plant | 2 x Offshore transformer stations & Onshore switchgear with SVC PLUS |
| Number of wind turbines | 140, each 3.6 MW |
A project 11 kilometers off the Kentish coast, consisting of one hundred 3.0 MW wind power units, produces electricity for Vattenfall UK. Siemens supplied the 33 kV / 132 kV offshore substation station for this project, equipped with two 180 MVA transformers, and the onshore substation including two SVC PLUS compensation systems. Siemens also ensured compliance with grid code, carried out performance studies, and provided the onshore cable system.
| Customer | Thanet Offshore Wind Ltd., U.K. |
| Project name | Thanet OWP |
| Location | North Sea, near the coast line of Kent, Foreness Point and Richborough, Kent |
| Power Rating | 300 MW |
| Voltage levels | 11 kV / 33 kV / 132 kV, AC |
| Equipment | 2 x SVC PLUS 2 x 180 MVA transformers (33/132 kV) 2 x 55 MVA transformers (11/33 kV) 2 x three-phase 132 kV XLPE submarine cables 2 x 132 kV HIS, 11 kV GIS Mechanical switched Capacitors and Reactors (MSR/MSC) |
| Type of plant | Offshore 33 kV / 132 kV transformer station & onshore substation with SVC PLUS |
| Number of wind turbines | 100, each 3.0 MW |
A few kilometers off the Lincolnshire coast 54 Siemens 3.6 MW wind turbines produce electricity for Centrica Renewable Energy Ltd. Two 100 MVA transformers are at the heart of the 33/132 kV onshore substation that receives the generated electricity through three 33 kV XLPE subsea cables. Siemens supplied the substation and the onshore cable system as well as grid, design, and performance studies for the wind farm.
| Customer | Centrica Renewable Energy Ltd., U.K. |
| Project name | Lynn / Inner Dowsing |
| Location | Greater Wash area, Great Britain national waters and Middle Marsh, UK |
| Power Rating | 180 MW |
| Voltage levels | 33 kV / 132 kV, AC |
| Equipment | 2 x 100 MVA transformers, 6 x threephase 33 kV XLPE submarine cables |
| Type of plant | 33 kV / 132kV onshore transformer station |
| Number of wind turbines | 54, each 3.6 MW |
About seven kilometers off the Swedish coast, 48 Siemens wind turbines, each with an output of 2.3 MW, produce electricity for Vattenfall AB, a leading Swedish power provider. The 33/138 kV Siemens substation with its 120 MVA transformer is located within the wind farm footprint. Power transmission to the onshore grid is accomplished with a three-phase 138 kV XLPE subsea cable connecting the wind farm with a substation in the town of Bunkerflo.
Siemens also performed extensive design and performance studies for the entire project.
| Customer | Vattenfall AB, Sweden |
| Project name | Lillgrund |
| Location | Oresund, Swedish National Waters and Bunkeflo (Sweden) |
| Power Rating | 110 MW |
| Voltage levels | 33 kV / 138 kV, AC |
| Equipment | 120 MVA transformers 1 x three-phase 138kV XLPE submarine cable |
| Type of plant | 33 kV and 138 kV Offshore transformer station |
| Number of wind turbines | 48, each 2.3 MW |
2011-May-06 | Text/Freigabe: M. Walz, U. Rohr