The test bays of the Schaltwerk Hochspannung Berlin open up a multitude of opportunities - from experiments on basic principles to type testing. The Schaltwerk Hochspannung (HV switchgear manufacturing plant) in Berlin is Siemens' technology center for the development and manufacture of high-voltage switchgear, gas-insulated high-voltage substations and surge arresters. The greatest of care is taken here to develop and manufacture quality products. In addition to proven methods of calculation, the engineers of the Development Department have at their disposal their own test bays equipped with the very latest in measuring and testing equipment. These are constantly being added to with new processes and methods that enhance the effectiveness of the bays, the scope of experiments and tests that can be conducted and the depth of information provided in the test results. The highly diversified range of test bays support all stages of development: from experimentation with basic principles, through initial testing of test units and checks on prototype breakers, to globally recognized type testing of first units for delivery. The beneficiaries of these exemplary development facilities at our in-house test bays are, when all is said and done, each and every plant operator who decides to purchase Siemens switchgear.
The following advantages ensue from the fact that we have our own test bays:
| High voltage test | |
| AC voltage | 1200 kV |
| Lightning impulse voltage | 3000 kV (also with combined voltage test) |
| Switching impulse voltage | 1800 kV (also with combined voltage test) |
| DC voltage | 600 kV |
| Switching test | |
| Output for direct test | 6400 MVA |
| Equivalent output for synthetic test | 104 GVA |
| Short-circuit current at 35 kV (RMS) | 120 kA |
| Impulse and short-time current, three-phase | 300 kA/120 kA, 3 s |
| Temperature-rise test | |
| 6 kA, single and three-phase | |
| 16 2/3 Hz up to 60 Hz | |
| Physics laboratory | |
| Performance test | up to 63 kA, 50/60 Hz direct and synthetic, up to 120 kV |
also with combined voltage test
The test bays at the Schaltwerk Hochspannung (HV switchgear manufacturing plant) in Berlin have been accredited according to ISO/IEC 17025. This means that Siemens satisfies an important prerequisite enabling it to be awarded product certificates recognized throughout the EU. Accreditation entails tests conducted on high-voltage switchgear and on items of power engineering equipment in accordance with relevant test specifications.
The test bays, as accredited facilities of the PEHLA association, are integrated in an international structure of testing and certification stations. The tests - and the documents compiled from the results of these tests - accordingly meet the highest requirements.