More than 30 years of wind power experience
Since 1980, the focus has been on developing competitive wind turbines. From the first 22-kW wind turbine up to the MW range turbines of today, the products have helped harnessing the power of wind.
Secure development requires specialist knowledge, and no other wind turbine manufacturer can match the specialist knowledge of Siemens Wind Power. Based on more than 30 years of continuous presence in the wind industry, we offer the best-skilled management and engineering staff – and the designs of any new product combine the accumulated experience of all the previous turbines with the latest advances in the fields of aerodynamics, structural dynamics, noise reduction and grid performance. The result is a reputation for high quality, logical and solid design and creative details that was founded with the first 22-kW turbines of 1980 and has continuously been increased since then. A reputation that is well-deserved by the MW range "workhorses" of today.The most important resource of Siemens Wind Power is undoubtedly the more than 8,000 employees - their experience, technical know-how and enthusiasm. An experienced management team vouches for continuity and confidence. We offer a unique mix of experience and innovation, wisdom and vision. A mix that makes Siemens Wind Power a reliable supplier and a dependable partner.
The large-scale wind power plants developed in recent years require significant project management know-how in order to be completed successfully. Siemens has extensive experience in this field and has, by the timely completion of hundreds of wind power plants, including the challenging offshore wind power plants, proven itself as a competent supplier of large, complicated projects.
Siemens Rotor Sync is an add-on feature to the Siemens Park Controller (SPC), which performs the regulation of turbines at wind farm level. The most important functions of the SPC are power control and voltage control. With the introduction of Siemens Rotor Sync, the SPC can now also utilize information about the rotation speed and rotor angle position of the individual turbines. Based on this input, each turbine’s rotation speed is adjusted to reach a state of synchronous rotation in order to create an atmosphere of elegance and harmony.
As Siemens wind turbines on an average basis are running with the same rotor speed from 7-8 m/s and above, only small adjustments to the speed reference is needed to keep the turbines in sync. The small adjustments are insignificant with respect to loads and power production. If synchronization is required at lower wind speeds, small reductions in energy output will occur, but such reductions are normally marginal compared with the total energy output.
A demonstration video of a synchronous wind farm versus a non-synchronous farm can be seen here.
IntegralBlade® - A key technology unique to the wind industry
All blades for Siemens wind turbine platforms with power ratings from 1.3 to 6.0 MW, and rotor diameters from 62 to 154 meters, are manufactured using the patented IntegralBlade® technology. The blades are made from fiberglass-reinforced epoxy resin, and their external design represents state-of-the-art wind turbine aerodynamics.
The IntegralBlade® technology invented by Siemens Wind Power allows the manufacture of single-piece wind turbine blades in a closed process. The fiberglass reinforcement is laid out to dry using a special molding arrangement with a closed outer mold and an expanding inner mold.
After completion of the fiberglass lamination process, the epoxy resin is injected under vacuum conditions. Then the blade, which is still enclosed in the mold, is hardened at high temperature. Finally, the blade is removed from the outer mold after the epoxy resin has hardened. The inner mold is collapsed with a vacuum and pulled from the blade. The result is a complete, seamless blade finished in a single process. A truly integrated success.
Shielding wind turbines against lightning
Protecting the entire wind turbine, the Siemens lightning protection system has helped avoid lightning strike related failures for decades.
The Siemens lightning protection system is designed to help protect wind turbines from the effects of direct and nearby strikes. Based on more than 30 years of wind power experience, the Siemens lightning protection system has shown excellent performance in wind turbine applications all over the world.
The lightning protection system is designed to help protect against lightning strikes in several ways. All main components including the nacelle, blades, controller and tower have extensive lightning protection integrated into their design.
The energy output of a wind turbine is dependent on the rotor size. With larger rotor sizes, higher production can be obtained. However, a bigger rotor traditionally increases the loads on the wind turbine, which calls for larger and heavier structural components. Siemens new aeroelastically tailored blade changes that.
The newly developed blade design couples controlled torsional twisting of the blade with aerodynamic loading. This ultimately provides improved performance at low wind speeds due to the larger rotor, and optimal load characteristics at all wind speeds.
The secret behind the aeroelastically tailored blade is to be found in the intelligent design work, which added a bend-twist-coupling within the blade, resulting in the blade reducing the loads on the turbine.
The new blade will instantly adjust the blade’s angle of attack created by wind gusts. This minimizes the stress on the turbine, whereas the pitch and turbine control system handles the slower variations in the wind speed for optimal operation. These properties represent major advances in blade performance and design.
The Siemens High Wind Ride Through application allows a wind turbine to operate at some storm-level wind speeds and is a breakthrough in stabilizing energy output.
High Wind Ride Through is an intelligent solution for both onshore and offshore wind turbines that enables more stable energy production.
When the wind speed is higher than 25 meters per second, wind turbines typically shut down in order to avoid overload due to extreme loads. Equipped with High Wind Ride Through, the wind turbine will gradually reduce power output instead of shutting down completely. This results in a more stable power output at high wind speeds.
As a result, the operating range of the wind turbine at high wind speeds is extended, while remaining load neutral. The wind turbine becomes more grid-friendly, as the amount of energy fed into the grid becomes more stable and predictable.
Higher towers significantly increase the energy yield of a wind turbine generator on sites with a high wind shear. At the same time, they pose considerable challenges in terms of transportability and costs. Siemens offers an innovative and economically viable tower concept to allow its wind turbines reach heights above 100 m.
The Bolted Steel Shell Tower consists of multiple tower sections, mounted on top of each other. Each section is made out of steel shells which are assembled together on site.
The steel shells are produced from bended steel plates and can be transported to site with standard trucks. They are bolted together with HRC (tension-controlled) bolts to form a tower section. The modular space concept of the Bolted Steel Shell Tower allows for very high hub heights (in excess of 140 m) with very low transportation requirements.
Siemens Turbine Load Control 2.0 (TLC®) actively controls the wind turbine loading based on real time operating conditions to maximize the annual energy production over the life of the wind power plant.
TLC® is an intelligent turbine control system which dynamically controls the wind turbine based on real time wind conditions allowing it to operate with only marginal or moderate reduction in power output in high load conditions.
When Siemens wind turbines are equipped with TLC®, some projects can utilize larger rotor diameters and help maximize the annual energy production without exceeding loads, and without the grid instability introduced by traditional sector management systems.
With traditional sector management, wind turbines will typically shut down at predefined conditions, such as occasional strong wind from certain directions. TLC® intelligently alters the control settings in accordance with the wind conditions and keeps the wind turbines in operation while remaining load neutral.
A reliable product and a well-run service organization help to ensure that wind turbines are a good investment. In addition to their strong and reliable basic construction, all Siemens turbines are accompanied by a comprehensive guarantee. This ensures that the customers know that their turbine will provide the best possible operational reliability both during the guarantee period and beyond.
Other languages