Gasification offers one of the cleanest and most flexible ways of converting coal, petcoke, refinery residues or other low-grade fuels into high-value products such as electricity, chemicals or clean transportation fuels. Combining gasification with advanced gas turbines in Integrated Gasification Combined Cycle (IGCC) power plants results in a highly efficient and environmentally friendly technology for coal-based power generation. Gasification based plants can easily include readily available technology for CO2 capture allowing the CO2 to be transported to oil fields for enhanced oil recovery or to a site for sequestration.
The entrained-flow Siemens Fuel Gasifier (SFG) is able to convert a wide range of solid or liquid carbonaceous fuels and is ideally suited for all ranks of coal from anthracite coal to lignite with high ash and moisture content. With more than 25 years of combined operating experience and innovative design features such as their unique cooling screen design and the efficient dry-feeding system, Siemens Fuel Gasifiers are a reliable solution for economic energy conversion.
Siemens is a collaborative and flexible OEM partner who is entirely committed to delivering tailored technology gasification solutions that are more reliable, more efficient, more competitive, and easier to maintain. According to the customer’s needs, Siemens provides all services from engineering the Gasifier Island to key equipment, project execution and service solutions.Siemens has a wide-range of proven technologies and the know-how to integrate them into comprehensive gasification based solutions capable of providing a reliable supply of synthesis gas for the production of products including power, chemical feedstocks and clean transportation fuels. Our Typical Scope of Supply Includes:
The Siemens Gasification Test Center is located at our headquarters in Freiberg, Germany and is one of the most comprehensive gasification test facilities in the world. More than 60 different fuels have been tested so far, which gives Siemens a rich body of experience. The centerpiece of the Siemens Gasification Test Center is a 5 MWth gasification reactor which is complemented by a range of feedstock preparation systems (both solid and liquid) and related gas cleaning process units. At the Siemens Gasification Test Center, a broad range of test conditions can be simulated. It is used to:
The Siemens Gasification Test Center also includes a test rig for high-pressure coal feeding. This test rig consists of a large-scale, fully equipped dry feeding system and can be used to optimize feeding solutions. In particular, it allows the following aspects to be explored:
| Owner/ Plant Name |
Country | Start up/ Project Status |
Feedstock | Units/Size | Final Prodct |
| SVZ Schwarze Pumpe | Europe | 1984-2007 | Lignite, natrual gas, tar oils, liquid waste | 1 x SFG-200 |
Methanol and Power (IGCC) |
| Sokolvska uhelna a.s. | Europe | operational | Liquid fixed-bed gasifier by-products | 1 x SFG-200r |
Power (IGCC) |
| Shenhua Ningxia Coal Industry Group Co., Ltd. | China | operational | Bituminous coal | 5 x SFG-500 |
Methanol / Polypropylene |
| China Power Investment (CPI) | China | Under construction | Chiness Sub-bituminous | 8 x SFG-500 |
Synthetic Natural Gas (SNG) |
| Ctl. Project/Ningxia | China | Under construction | Bituminous coal | 24 x SFG-500 | Transportation Fuels |
| Shanxi Lanhua Coal Chemical | China | 2 SFG-500 gasifier shipped | Anthracite | 2 x SFG-500 |
Ammonia/Urea Fertilizers |
| Secure Energy, Inc. | USA | 2 SFG-500 gasifiers shipped | IL Bituminous coal |
2 x SFG-500 |
Transportation Fuels |
| Texas Clean Energy Project | USA | Financial Close End 2012 | Lignite | 2 x SFG-500 |
Power (IGCC) Ammonia /Urea/Fert. |
| Tenska Inc. | USA | Engineering completed; project abandoned | Hard coal | 2 x SFG-500 |
Power (IGCC) and SNG |
| Captital Power Corp. | Canada | Engineering completed; project abandoned | Sub-bituminous coal | 1 x SFG-500 |
Power (IGCC) |
| AEC Australian Energy Comp. | Australia | Agremments signed: project abandoned | Lignite | 2 x SFG-500 |
Ammonia / Urea / Fertilizers |