Cables of the type PROTOFLEX EMV which have been manufactured in a 2nd source production site in between 1996 and mid 1999 may have severe quality problems. However to our actual knowledge this quality problem has occurred in parts of the production lots only.
Possibly affected cables have been supplied via Siemens sales channels and particular wholesalers to customers worldwide in the time range from 1996 until approx. 2001. These types of cables are used specifically for power supply connections of electrical motors to frequency converters (variable speed drives) in industrial applications, e.g. crane or machine tool applications.
We are talking about the entire type range of the
cable series, which were procured from an external supplier between 1996 and mid-1999 and then built into industrial installations of Siemens customers.
Generally, all kinds of industrial installations equipped with variable-speed drives may be affected, for example in the machine tool industry, in power generation, in power distribution switchgear, in industrial production, and in conveying and hoisting gear systems. Worldwide, Siemens is currently reviewing the technical details and the scope of possibly affected systems.
Due to possible omission of a metal deactivator in the polymer insulation of the phase conductors in these cables, they may age prematurely, therefore no longer meet prescribed functional and protection regulations. In the worst case, this could lead to direct short-circuits against which, however, technical protection is provided. Creepage currents can occur and may lead to smoldering or burning fires. There is the possibility that serious personal injury could occur.
The relevance of the situation became clear to Siemens in October 2006 after the discovery of non-conforming cables in a European industrial plant. So far we have not heard of any injuries to people nor of any damage to property.
We cannot specify the exact number of totally affected customers at the moment. To date we have identified around 15 customers. Siemens is checking the sales and marketing channels for the relevant period to ascertain whether more customers might have been supplied with imperfect products. For this reason the Siemens sales network worldwide has been instructed to immediately contact any customers who may be potentially affected in order to clarify the situation.
As soon as Siemens learned of the cable situation, it immediately informed all known affected customers to date thereof, issued instructions on safety precautions to be taken and communicated measures for checking the installed cables. In the context of a duty to inform (prescribed by statute and commercial law), each customer we identify will be individually notified immediately. Appropriate corrective measures for each situation will be implemented.
We have known about it since October 2006. We immediately took action to assertain the extent of the potential problem, find out which customers may be affected and inform them.
The circumstances require that the extent of the deliveries first be ascertained and affected customers informed and instructed how to identify the potentially problematic cables. Affected customers around the world will be specifically notified directly through our sales channels. For this reason, our worldwide sales network is currently busy contacting those customers who might have been supplied with the aforementioned cables during the time period in question. A public notification/recall campaign through relevant trade journals is being prepared.
The statutory regulations in the respective countries to which the cables concerned were delivered and the individual contractual provisions apply here. To our current knowledge, deliveries from the production period from 1996 to 1999 are no longer under prescribed or statutory warranty. Siemens is not therefore under any general warranty obligation to replace cables from the aforementioned delivery period. Nevertheless, we want to support affected customers by supplying replacement cables. Siemens regards this as its duty in maintaining quality standards towards its customers.
We cannot say at the moment.
The statutory regulations in the respective countries to which the cables concerned were delivered and the individual contractual provisions apply here.
However, Siemens wishes to support its customers and is nonetheless offering replacement of the cables affected.
This is still subject to investigation. However, our present knowledge indicates Siemens Automation & Drives (A&D), Industrial Solutions and Services (I&S), Medical Solutions (Med), Power Generation (PG), Power Transmission and Distribution (PTD), Siemens Building Technologies (SBT) and Transportation Systems (TS) are affected.
One can never completely exclude the possibility that, despite tight-knit quality assurance measures, potential quality issues may become evident over time. Despite rigorous product observation by our quality assurance departments, the first visible irregularities have only appeared recently – due to the aging process of the cables, which depends on several factors – after around two years of operation.
There are no gaps in our quality control, and we have reacted both quickly and suitably in the relevant cases
Non-conforming products always carry the risk of loss of image; however, we do not expect our image to be harmed by this case due to the open and prompt manner in which we have dealt with it. On the contrary, we hope that the measures proactively agreed with each and every customer will serve to consolidate their trust in Siemens