Siemens has used its great experience and know-how in network planning to develop powerful system simulation and analysis tools to assist engineers in their highly responsible work. The software tools of the Power System Simulator PSS®Product Suite are leading products with respect to technical performance and user-friendliness. Comprehensive interfaces enable the interaction of all PSS®Product Suite tools, and also support the integration with other IT systems.
Please follow the links to our software support pages or support request forms.

PSS®E is the premier software tool used by electrical transmission participants world-wide. The probabilistic analyses and advanced dynamics modeling capabilities included in PSS®E provide transmission planning and operations engineers a broad range of methodologies for use in the design and operation of reliable networks. PSS®E is the standard Siemens offering for electrical transmission analysis that continues to be the technology of choice in an ever-growing market that exceeds 115 countries.
Since its introduction in 1976, the Power System Simulator for Engineering tool has become the most comprehensive, technically advanced, and widely used commercial program of its type. It is widely recognized as the most fully featured, time-tested and best performing commercial program available.
PSS®E is an integrated, interactive program for simulating, analyzing, and optimizing power system performance. It provides the user with the most advanced and proven methods in many technical areas, including:
PSS®E Version 33 released May 2011.
PSS®E high-performance transmission planning software has supported the power community with meticulous and comprehensive modeling capabilities for more than 40 years. Built on proven technology, Siemens PTI launches PSS®E Version 33 with new features and enhancements to improve your work flow, support grid code compliance and provide preventative security capabilities.
Version 33 introduces several new forms of analysis that includes Preventive Security Constrained OPF and N-1-1 contingency analysis. A number of new analytical models have been added along with the standardization of the Dynamic CONEC and CONET type models, improvements to data entry and connection codes in Short Circuit, an updated fully integrated Scenario Manager as well as improvements to basic power flow and dynamic simulation activities.
As requested by the user community, Version 33 includes a native induction machine model which can be used for an accurate representation of induction motor type modes throughout the PSS®E engine.
Sensitivity analysis is a method to systematically study the impacts of changes in system operation conditions such as MW and MVar power injections on changes in branch flows and bus voltages. The function can calculate sensitivity factors with either a DC linear network or full AC network and can be used in the following applications:
System security is the ability of a system to withstand contingencies, in other words, to remain intact even after equipment outages or failures. The Security Constrained Optimal Power Flow (SCOPF) can be used to perform a secure control to ensure the system security. It is a special class of OPF problems which takes into consideration the system constraints of predefined contingencies. The preventive method enables the system to be prepared for certain contingencies beforehand, and it does not take into account the system’s post-contingency control capabilities.
The N-1-1 contingency solution performs an AC power flow to solve the primary contingency, applies the appropriate system adjustments in accordance with one of three adjustment modes, and then runs another AC power flow to solve the secondary contingency. The three modes are local control, corrective action and Preventive Security Constrained Optimal Power Flow (PSCOPF). Under each mode, several types of controls are available to adjust the system to meet the specified goals.
Provision has been made to call every PSS®E dynamic model from within PSS®E without the need for an explicit call statement in the connection routines (CONEC and CONET.) As a result of this change, no model in the PSS®E supplied library would require any compilation or linking of the connection routines. CCT models, a new family of models, have been introduced to replace the old CONEC and CONET type models. By using the new CCT models, in place of the old CONEC-CONET type models, users will be able to prevent user models from being called in the CONEC and CONET subroutines and thereby avoid compilation and linking of these routines.
Click here to download the PSS®E 33 Release Notes for information on these features and more.
In recent years, major blackouts around the world have increased awareness regarding the benefits of accurate modeling for improved system planning. Municipalities and cooperatives that have traditionally relied on regional independent system operators (ISO) or transmission owners (RTO) to provide planning modeling, need to be actively involved to ensure the accuracy of their own system representation. To streamline the process of exchanging data with their ISO, RTO, or other governing body, utility companies, municipalities and cooperatives need a solution to perform essential tasks in a cost-effective manner.
To address these challenges Siemens PTI offers PSS®E Xpress. Derived from our market-leading PSS®E transmission planning software and a 40-year heritage, PSS®E Xpress includes essential functions for modeling and data exchange.
Model and analyze your network for less than $11 a day!
The PSS®E Xpress power flow toolbox will make your day-to-day tasks easier:
Compile trustworthy models with proven technology.
Built upon the proven success of PSS®E, PSS®E Xpress has:
Speak the same language to avoid conversion or translation errors.
PSS®E Xpress enables you to:
Use an intuitive Windows® based solution developed by engineers for engineers!
Siemens PTI offers a number of fast and convenient ways to become a PSS®E Xpress expert!
For an additional $5.50 USD per day then PSS®E Xpress Plus is your solution!
PSS®E Xpress provides the answers!
Power system planning and analysis tools have become a necessity for organizations through out the electric power industry to address escalating complexity in modern transmission network systems.
With an escalating need for graduate engineers practiced in applying planning tools and to prepare graduates for a career in the complex competitive environment of network planning, Siemens PTI is pleased to provide educators and students with a dual approach to learning and applying the software tool of choice for over 11,000 professionals at 885 companies in 117 countries.
PSS®E University edition- A means to provide the fundamentals of power engineering
PSS®E University edition reinforces your course studies and provides students with the fundamentals needed to enter the workforce. Presenting students with actual problems that network planning engineers face today and allowing them to work towards a solution, gives students the analytical experience they will need in the power system environment. With the integration of PSS®E being so prevalent, and PSS®E University edition offering the same capabilities as our commercially licensed product, students will have an advantage of being pre-exposed to the software before entering the workforce. The PSS®E University edition includes the following components:
For graduate level studies and pursuit of external government funded research, Siemens PTI recommends educators consider the use of our commercially licensed product at a special price of:
This special offer includes the following PSS®E components:
For details on previous events, click here.
The United Kingdom & Ireland Regional PSSE Users Forum was held in Manchester, U.K. on January 19, 2012.
The Asia/Pacific Regional Users Group Meeting scheduled to be held in Chiang Mai, Thailand on February 13-17, 2012 has been cancelled.
The U.S. Southern Regional Users Group Meeting will be held in New Orleans, Louisiana on April 16-20, 2012. Click here for more details.
The European Regional Users Group Meeting will be held in June 2012. Further details to follow.
The US Northern Regional Users Group Meeting will be held in Minneapolis, Minnesota on September 17-20, 2012. Further details to follow.
The China Regional Users Group Meeting will be held in October 2012. Further details to follow.
The Africa Regional Users Group Meeting will be held in December 2012. Further details to follow.
San Antonio, Texas
Jan. 24, 2012- Jan. 26, 2012
San Diego, California
Booth 1431
March 6-9, 2012
San Diego, California
July 22, 2012- July 26, 2012
Enter our User Support Area for technical support or contact us.